Skip to main content
infoinfo982
Associate
Apr 14, 2026 2:35 PM UTC
Solved

Ethernet 10Base-T1S on the STM32C5

Hi,

On the stm32c5 nucleo board (NUCLEO-C5A3ZG) there is T1S OA PMD driver (not mounted?).  In the header file 

"stm32c593xx.h" exists a 10BASE-T1S control register "MAC10BT1SCR". 

But there is no documentation in the Reference Manual RM0522 Rev 1, and I can't find a way to enable T1S on MXcube2.

Can anyone help me here? Is the T1S PDM really integrated in the C5 series?

I would really like to experiment with 10Base T1S.

Regards

Patrick

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 14, 2026 7:51 PM UTC

Issue internally confirmed. No T1S support on STM32C5.

All T1S mentions will be removed from the STM32C5 package.

Thank you for your contribution.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

7 replies

Andrew Neil
Super User
Apr 14, 2026 2:46 PM UTC

@infoinfo982 wrote:

I would really like to experiment with 10Base T1S.


Me too!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
Apr 14, 2026 4:00 PM UTC

Hello,

Since there is no indication in the documentation the product supports the T1S, it doesn't support it. I will escalate it internally to double check. Internal ticket for follow-up CDM0061715 (not accessible by the community users).

For the T1S PHY footprint on the board it may be used for another product.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Pavel A.
Apr 14, 2026 5:02 PM UTC

Quick googling shows that 10BASE-T1S specifies only the PHY. So the MAC of STM32C5 should work with any compatible PHY. Why does it have the 10BASE-T1S control register "MAC10BT1SCR" ?

DS15137 has no notion of 10BASE-T1S in ETH section.

Andrew Neil
Super User
Apr 14, 2026 5:24 PM UTC

@infoinfo982 wrote:

In the header file "stm32c593xx.h" exists a 10BASE-T1S control register "MAC10BT1SCR". 


Please show that section of that file.

 

How to insert source code

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 14, 2026 7:51 PM UTC

Issue internally confirmed. No T1S support on STM32C5.

All T1S mentions will be removed from the STM32C5 package.

Thank you for your contribution.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
ST Technical Moderator
Jun 25, 2026 10:05 AM UTC

Hello ​@infoinfo982 

The issue has been solved in the new STM32C5 Ecosystem release 2.1.0. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om