Skip to main content
shark
Associate III
Dec 17, 2013 9:26 AM UTC
Question

ETH_Start() sometimes failed to start mac

Posted on December 17, 2013 at 10:26

Hi

My product is based on stm32f407, the Ethernet works well normally, except that, sometimes(10% possibility) after the MCU powered up or hot rebooted, the mac can transmit packets, but can NOT receive. 

When this problem happened, I checked status inside chip, (all the register values listed at bottom):

1. The value in MMCTGFCR indicate tx is good, I can see the packet by wireshark.

2. but MMCRGUFCR is always 0, the RX interrupt does not come too.

3. the magic is here, current value in MACCR is:

    40028000      MACCR = 0000800c

   I write the SAME 0000800c into 40028000 again manually, the whole MAC works! and always this way.

My ethernet driver is:

 waiting for ethernet negociation finished

 ETH_Init()  // according to speed, ...

 ETH_Start()

 ETH->MMCCR = ETH->MMCCR;  // this patch helps, but not reliable

ETH_Start() failed to start the state machine? I dont konw how to check it or patch it. MMCCR's TE and RE bit is magic, no time requirement?

==============

eos % int -v eth0

eth0       line UP, protocol UP

           Link encap Ethernet MTU 1500 Link addr 00:01:02:03:04:72

           IP addr 192.168.1.114 netmask 0xffffff00, broadcast 192.168.1.255

           sent: ip 4 tot 5 idle 5? qlen 0

           recv: ip 0 tot 0 idle 1?37?

phy:

reg[ 0]=1000

reg[ 1]=782d

reg[ 2]=0007

reg[ 3]=c0f1

reg[ 4]=05e1

reg[ 5]=0020

reg[ 6]=0000

reg[ 7]=ffff

reg[ 8]=ffff

reg[ 9]=ffff

reg[10]=ffff

reg[11]=ffff

reg[12]=ffff

reg[13]=ffff

reg[14]=ffff

reg[15]=0000

reg[16]=0040

reg[17]=0002

reg[18]=00e0

reg[19]=ffff

reg[20]=0000

reg[21]=0000

reg[22]=0000

reg[23]=0000

reg[24]=ffff

reg[25]=ffff

reg[26]=0000

reg[27]=000a

reg[28]=0000

reg[29]=00c0

reg[30]=00d0

reg[31]=1044

reg[32]=1000

PHY_status 3: 10M half

===tx desc ===

 ♯  address   status     size buf1addr nextdesc

00 2001dea0 00100000 00000000 2001dec0 2001c000

01 2001c000 30100000 0000003c 2001c020 2001c620

02 2001c620 30100000 0000003c 2001c640 2001cc40

03 2001cc40 30100000 0000003c 2001cc60 2001d260

04 2001d260 30100000 0000003c 2001d280 2001d880

05 2001d880 30100000 0000003c 2001d8a0 2001dea0

===rx desc ===

 ♯  address   status     size buf1addr nextdesc

00 2001e4c0 80000000 00004600 2001e4e0 2001eae0

01 2001eae0 80000000 00004600 2001eb00 2001f100

02 2001f100 80000000 00004600 2001f120 2001f720

03 2001f720 80000000 00004600 2001f740 2001e4c0

mac

40028000      MACCR = 0000800c

40028004     MACFFR = 00000040

40028008    MACHTHR = 00000000

4002800c    MACHTLR = 00000000

40028010   MACMIIAR = 00000010

40028014   MACMIIDR = 00001000

40028018     MACFCR = 00000080

4002801c  MACVLANTR = 00000000

40028028  MACRWUFFR = 00000000

4002802c  MACPMTCSR = 00000000

40028038      MACSR = 00000000

4002803c     MACIMR = 00000000

40028040    MACA0HR = 80007204

40028044    MACA0LR = 03020100

40028048    MACA1HR = 0000ffff

4002804c    MACA1LR = ffffffff

40028050    MACA2HR = 0000ffff

40028054    MACA2LR = ffffffff

40028058    MACA3HR = 0000ffff

4002805c    MACA3LR = ffffffff

mmc

40028100      MMCCR = 00000000

40028104     MMCRIR = 00000000

40028108     MMCTIR = 00000000

4002810c    MMCRIMR = 00020060

40028110    MMCTIMR = 0020c000

4002814c MMCTGFSCCR = 00000000

40028150 MMCTGFMSCCR = 00000000

40028168   MMCTGFCR = 00000005  // tx is good, I can see it by wireshark too

40028194  MMCRFCECR = 00000000

40028198  MMCRFAECR = 00000000

400281c4  MMCRGUFCR = 00000000

dma

40029000     DMABMR = 02c16080

40029004    DMATPDR = 00000000

40029008    DMARPDR = 00000000

4002900c   DMARDLAR = 2001e4c0

40029010   DMATDLAR = 2001c000

40029014      DMASR = 00660404

40029018     DMAOMR = 06202002

4002901c     DMAIER = 00010040

40029020  DMAMFBOCR = 00000000

40029024   DMARSWTR = 00000000

40029048   DMACHTDR = 2001dea0

4002904c   DMACHRDR = 2001e4c0

40029050  DMACHTBAR = 2001dec0

40029054  DMACHRBAR = 2001e4e0

#mac-driver
    This topic has been closed for replies.

    5 replies

    shark
    sharkAuthor
    Associate III
    Dec 20, 2013 2:27 AM UTC
    Posted on December 20, 2013 at 03:27

    This problem happens on 10M half duplex ethernet hub.

    I tested it again on 100M full ethernet for 100 times, never happens.

    So, my software driver should be no problem. Hope ST engineers to test driver on 10M ethernet too.

    I guess, MACCR's start bits must have timing requirement. but what is it? or,

    even when the bit is 1, writing 1 again will trigger some internal actions again, so where is the status bit to indicate it is realy started.

    francescatodiego
    Associate III
    Dec 20, 2013 4:15 PM UTC
    Posted on December 20, 2013 at 17:15

    I wrote my

    driver

    for

    ethernet

    STM32F4

    I had the same

    problem

    using this enable sequence

    ETH-

    >

    MACCR

    |

    =

    ETH_MACCR_RE

    ;

    ETH-

    >

    MACCR

    |

    =

    ETH_MACCR_TE

    ;

    sometimes (

    I do not know

    why

    )

    the device

    was not working

    writing instead

     

    ETH-

    >

    MACCR

    |

    = (

    ETH_MACCR_RE

    |

    ETH_MACCR_TE

    );

    always works

    ...

    but

    do not ask me

    why

    shark
    sharkAuthor
    Associate III
    Dec 27, 2013 1:13 AM UTC
    Posted on December 27, 2013 at 02:13

    It works well after modified as you suggested.

    thank you

    Tesla DeLorean
    Guru
    Dec 27, 2013 3:06 AM UTC
    Posted on December 27, 2013 at 04:06

    Thanks for the update, btw what PHY's are you guys using in these applications?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    francescatodiego
    Associate III
    Dec 27, 2013 4:55 PM UTC
    Posted on December 27, 2013 at 17:55

    I work with wvshare STM32F4 devboard (OPEN407I)

    The board kit include also an ETH interface with PHY DP83848.