Skip to main content
jlchoobs
Associate III
July 24, 2012
Question

Etching Brds - USB Prob - Solution Found

  • July 24, 2012
  • 18 replies
  • 2835 views
Posted on July 24, 2012 at 20:15

I am building my own stm32f4 boards. The code runs, but I cant get the USB to be recognized by windows - just Device-Not-Recognized. But the same code works on my DemoBoard.

I followed the DemoBoard Schem except for the EMID02USB03F2 chip.

USB connected as :

PA9 - UsbVbusP1

PA11 - /\/\ - UsbDmP2 (res=20R)

PA12 - /\/\ -UsbDpP3 (res=20R)

PA10 - UsbIdP4

GND - UsbGndP5

I still do not have the USB working on my own Boards (while it does work on the Demo Board). And, I followed the Demo Brd Schem explicitly.

Except that I did not add the EMID02USB03F2 chip. Is this neccessary ? - It was not suggested in the Specs.

Anybody have any useful ideas ?

0690X0000060MlmQAE.gif

    This topic has been closed for replies.

    18 replies

    jlchoobs
    jlchoobsAuthor
    Associate III
    July 26, 2012
    Posted on July 26, 2012 at 07:15

    STM32 Manuals and Schematics CORRECTION - USB Pinout Backwards

    In Manufacturing my own Boards, and with the assistance of Tsuneo,

    I have found that the SPECS specify the USB PINOUT Backwards.

    This is afterI analyzed the Specs and Schems

    - which match my Eagle Pcb Files and my Boards.

    And, I tested this from Cable-end to Micro-Pins with a MultiMeter.

    The UsbVBus+ and UsbGND are Correct,

    but the UsbDm and UsbDp are specified BACKWARDS

    in both Stm32F4_Ref Manual and the Discovery Board Schems.

    No, you can not just flip the cable - Only TWO of the PINS are Backwards.

    PINOUT CORRECTION below :

      p1=UsbVBUS -> PA9

      p2=UsbDM     -> res=20R ->  PA12  (not PA11)

      p3=UsbDP      -> res=20R ->  PA11  (not PA12)

      p4=UsbID       -> PA10

      p5=UsbGND   -> GND

    -> Take HEED of this NOTE CORRECTION before making Boards !

    ------------------------------------------------------------------

    Tsuneo,

    You are kidding me.  I see the results as you say.  So the schematics are backwards ?

    Yes, I use USB-View, besides a Usb packet logger analyzer.

    Let me check the Usb connections.

    I forgot about this simple issue.  For example, just Google for USB PLUG PINOUT IMAGE , then click the images page.  Notice that the Plug on the Right is labeled Gnd D- D+ V+ , which should be Gnd D+ D- V+.  This error has been on there for years like this - and is still there. 

    Bingo ! - That fixes it.

    So, looking at the Stm32f4Discovery and Stm3240g and Stm32405_RefMan. 

    And scanned over my Eagle Pcb Files which match the Schems and Spec.

    -- It seems that they have the Pinouts backwards !

    I followed these Pinouts - but they are backwards - CORRECTION below :

    p1=UsbVBUS -> PA9

    p2=UsbDM     -> res=20R ->  PA12  (not PA11)

    p3=UsbDP      -> res=20R ->  PA11  (not PA12)

    p4=UsbID       -> PA10

    p5=UsbGND   -> GND

    Sounds ridiculous that this Error went through the Manuals and specs,

    - but I have seen it before.

    Explains why I have not seen and I can not find Schems and DIY Projects for the STM32 with USB.

    Tsuneo, thanks - for the unique and constructive idea and solution.

    --------------------------------------------------------------------------------

    From: chinzei.tsuneo

    Connection from the D+/D- pins of the USB receptacle to the MCU USB DP/DM pins may be swapped.

     ConnectionStatus: DeviceFailedEnumeration

     Device Bus Speed:      Low   <----------

    If the stm32f4 (Unknown device) is detected as low-speed, the D+/D- connections are swapped.

     

    mk299
    Associate III
    July 26, 2012
    Posted on July 26, 2012 at 11:25

    Would you mind to post a screenshot of your original schematic? Maybe it would help to clarify the problem.

    frankmeyer9
    Associate III
    July 26, 2012
    Posted on July 26, 2012 at 11:53

    So for the Nonsense Posting members - seems that following To-The-Spec is Wrong.

     

    Post your Nonsense somewhere else ...

     

    Just stop asking nonsense questions.

    jlchoobs
    jlchoobsAuthor
    Associate III
    July 26, 2012
    Posted on July 26, 2012 at 13:44

    Whats left for me to list ?

    Just look in the Manuals yourself that I listed: Stm32f4Discovery_Board_Manual Schem at end, and Stm32f405_Ref_Man fig 343 on page 934.  The Pinouts do not function hooked up this way - DM and DP need be reversed PA12 and PA11.

    I tested this from cable end to Micro Pins to UsbDM and UsbDP pins are specified backwards.
    cm600
    Associate II
    July 26, 2012
    Posted on July 26, 2012 at 15:22

    It is working for me :) PA.11 D- PA.12 D+

    See attachment for SCH.

    ________________

    Attachments :

    BB.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtUM&d=%2Fa%2F0X0000000aQj%2FuNfQQfpm6rl6vsIs0CCsZf.vm2Ov4_lF4ua3LB3WsL0&asPdf=false
    Tesla DeLorean
    Guru
    July 26, 2012
    Posted on July 26, 2012 at 16:44

    It is working for me :) PA.11 D- PA.12 D+

    Here too, and the ST-LINK USB connector is demonstrably connected PA11 DM, PA12 DP of the STM32F103's on several different discovery designs and matches the schematic. I haven't drunk enough Kool-Aid this morning to go pull uDFN packages off the board.

    Everyone needs to do their own due diligence, but I'm not buying into this conspiracy nonsense.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    mk299
    Associate III
    July 26, 2012
    Posted on July 26, 2012 at 20:19

    I did exactly what you supposed me to do and looked into the manuals (DM00039084 & DM00031020 and the datasheet DM00037051), but I was not able to reconstruct your problem. I can't see any error there.

    When I read the following sentence from [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32 Manuals and Schematics CORRECTION - USB Pinout Backwards&currentviews=49]your first post in this thread:

    <cite>

    I forgot about this simple issue.  For example, just Google for USB PLUG PINOUT IMAGE , then click the images page.  Notice that the Plug on the Right is labeled Gnd D- D+ V+ , which should be Gnd D+ D- V+.  This error has been on there for years like this - and is still there.

    </cite>

    I guess that you switched the pinout of your connector according to one of the several wrong images like, e.g.

    http://www.google.de/imgres?imgurl=http://wiki.bemaniso.ws/w/images/e/e9/USB_A_pinout.jpg&imgrefurl=http://wiki.bemaniso.ws/wiki/How_to_make_parallel_adapters&h=145&w=205&sz=9&tbnid=7dep87ZBSKq7zM:&tbnh=93&tbnw=132&prev=/search?q%3DUSB%2BPLUG%2BPINOUT%2BIMAGE%26tbm%3Disch%26tbo%3Du&zoom=1&q=USB+PLUG+PINOUT+IMAGE&usg=__L7a6hjObFHnWTITJT2_x0cCftlI=&docid=BgWv1IMT7sfFBM&sa=X&ei=cYMRUPXyMojbsgb2rYD4AQ&ved=0CGMQ9QEwAg&dur=587

    , instead of using a more trustful source as for example

    http://en.wikipedia.org/wiki/Universal_Serial_Bus#USB_standard_connectors

    or

    http://www.usb.org/developers/docs/usb_20_071012.zip

    .

    Because of this I asked for a screenshot of your schematic.

    jlchoobs
    jlchoobsAuthor
    Associate III
    July 26, 2012
    Posted on July 26, 2012 at 21:54

    What conspiracy - Bugs just happen ...

    Maybe it is backwards on the Board.

    I was refering to a later Design File v1065 , while the Printed File is v945.

    I think that I had swapped the pins after they were printed in design.

    Usb is on the Bottom of the Board and I probably got them backwards.

    Thanks for the help - for the members who did the research.