Skip to main content
Associate
May 15, 2024
Question

Error Transmitting data via UART when using ADC & DMA (works separately)

Hi All,

I have been a little confused about my code and would appreciate some help greatly...

I have a basic program where I would like to read the ADC values from a sensor, and transmit them via UART for later signal processing and whatnot.

The structure is simple, and when I tested out reading the values from the ADC, as well as sending strings via UART - they both work perfectly fine. But now when I merge the two, the UART does not work anymore... I do not see anything in my serial monitor (Putty)

I feel like I am missing something big, but cannot find it. I would appreciate it if someone pointed me in the right direction :)

in my main, I have: 

 

 

uint32_t value[2]; // start adc in DMA mode
int isSent = 1;
uint8_t tx_buffer[] = "Welcome to BinaryUpdates!\n\r"; 

int main(void)
{
 HAL_Init();
 SystemClock_Config();
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_ADC1_Init();
 MX_TIM3_Init();
 MX_TIM4_Init();
 MX_TIM2_Init();
 MX_USART6_UART_Init();

 HAL_ADC_Start_DMA(&hadc1, value, 2);

 while (1)
 {
	 if (isSent == 1)
	 {
	 	 HAL_UART_Transmit_DMA(&huart6, tx_buffer, 27);
// HAL_UART_Transmit_DMA(&huart6, value[0], sizeof(value[0]));
	 	 isSent = 0;
	 }
	 HAL_Delay(1000);
 }
}
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
	isSent = 1;
}

 

 

This topic has been closed for replies.

16 replies

Andrew Neil
Super User
May 15, 2024

@ponuliukas wrote:

the UART does not work anymore... 


What do you mean by that?

  • It transmits nothing at all ?
  • It transmits something, but not what you wanted ?
  • other ?

 

EDIT:

You haven't shown your definition of isSent, but it should be 'volatile'

Do you have any conflicts between ADC and UART pins?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
May 15, 2024

Thank you for the reply @Andrew Neil and @raptorhal2 , and apologies for not being perfectly clear. I edited the question :) 

Andrew Neil
Super User
May 15, 2024

It's confusing to edit the question after people have already commented on the question in its original form!

It's better to post an update as a reply.

Again,  isSent should be 'volatile'

 


@ponuliukas wrote:

the UART does not work anymore... I do not see anything in my serial monitor (Putty) 


That could be because your UART is sending something that's not visible to PuTTY ?

Have you check on the wires with a logic analyser or oscilloscope?

You're ignoring the return value from HAL_UART_Transmit_DMA - it might be telling you something ...

https://community.st.com/t5/stm32-mcus-boards-and-hardware/hal-rcc-oscconfig/m-p/674455/highlight/true#M19028 

What happens if you do away with the DMA, and just use a plain blocking send?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
raptorhal2
Lead
May 15, 2024

Edit: Cancel - I misunderstood. How do you get "value" into tx_buffer ?

Andrew Neil
Super User
May 15, 2024

@ponuliukas wrote:

 

 

uint8_t tx_buffer[27] = "Welcome to BinaryUpdates!\n\r"; 

 

 


Although it doesn't matter in the code you've shown so far, note that this does not leave space for a terminating NUL - so that won't be a proper C string.

To have a proper C string:

 

uint8_t tx_buffer[] = "Welcome to BinaryUpdates!\n\r"; 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.