Question
Error: Sector erase operation has failed — STM32G0B1CCT6
- 1 reply
- 575 views
Hello,
I am working with the STM32G0B1CCT6 MCU and facing an issue while flashing firmware using ST-LINK.
During the flashing process, I get the following error:
Error: Sector erase operation has failed at least for one of the existing specified sectors. Please verify flash memory protection. Warning: Connection to device 0x467 is lost
I have checked my hardware connections, and power supply seems fine. However, the erase operation still fails, and the device disconnects.
Could this be due to flash write protection, or some RDP (Readout Protection) setting?
Please help me resolve this issue.
I am attaching the screenshot of the error and the related project/file for reference.
Thank you!