Skip to main content
Julien FAUCHER
Associate III
March 23, 2018
Question

ERROR REPORT - STM32H7x3 Reference manual : GPIO MODER

  • March 23, 2018
  • 1 reply
  • 504 views
Posted on March 23, 2018 at 22:30

Hi,

In the reference manual for the STM32H7x3 RM (RM0433) the register map for the GPIO in the GPIO register map (p.500) appear to be incorrect :

  • For the GPIOA, based on H7 Headers it's actually MODERx and not MODEx
  • For GPIOx : There is that 'MODEv1' bit which is also false (MODER).

Then, those three rows may be merged into one single row (excepted that the initial values aren't the same)

Best regards,

Julien FAUCHER♯

#stm32h7 #error #bug #documentation
This topic has been closed for replies.

1 reply

Nesrine M_O
Associate
March 26, 2018
Posted on March 26, 2018 at 11:40

Hi

FAUCHER.Julien

,

Thank you for bringing these typos to our attention! It is noted and will be fixed in coming release of thedocument.

-Nesrine-