Error: registers may not be the same -- strexb r3,r2,[r3]'
- 7 replies
- 855 views
Hi,
I am currently using the following microcontroller (STM32F100C8T6B) in my design. I am using the STM32CubeIDE and I trying to build the project, but I am getting the following compiler errors from the "core_cm3.c" file
Error: registers may not be the same -- strexb r3,r2,[r3]'
Error: registers may not be the same -- strexh r3,r2,[r3]'
Any help would be greatly appreciated
Thanks,
WJ
This is the version for core_cm2.c
/**************************************************************************//**
* @file core_cm3.c
* @brief CMSIS Cortex-M3 Core Peripheral Access Layer Source File
* @version V1.30
* @date 30. October 2009
*
* @note
* Copyright (C) 2009 ARM Limited. All rights reserved.
Below is where the error in the file
/**
* @brief STR Exclusive (8 bit)
*
* @param value value to store
* @param *addr address pointer
* @return successful / failed
*
* Exclusive STR command for 8 bit values
*/
uint32_t __STREXB(uint8_t value, uint8_t *addr)
{
uint32_t result=0;
// register uint32_t result asm ("r2");
__ASM volatile ("strexb %0, %2, [%1]" : "=&r" (result) : "r" (addr), "r" (value) );
return(result);
}
/**
* @brief STR Exclusive (16 bit)
*
* @param value value to store
* @param *addr address pointer
* @return successful / failed
*
* Exclusive STR command for 16 bit values
*/
uint32_t __STREXH(uint16_t value, uint16_t *addr)
{
uint32_t result=0;
register uint32_t result asm ("r2");
__ASM volatile ("strexh %0, %2, [%1]" : "=&r" (result) : "r" (addr), "r" (value) );
return(result);
}