Skip to main content
TDK
October 23, 2019
Question

Error/omission in RM0090: missing CC4NP bit definition

  • October 23, 2019
  • 1 reply
  • 690 views

The CC4NP bit in the TIMx_CCER register should be listed in the reference manual in the section "17.4.9 TIM1 and TIM8 capture/compare enable register (TIMx_CCER)". Currently, only the CC1NP, CC2NP, and CC3NP bits are listed. The sections for the other timers correctly list this bit.

This bit is used when channel 4 is configured in input capture (IC) mode to help determine if triggers occur on rising and/or falling edges.

I checked the latest RM0090 (rev18) reference manual and the bit is not listed in there in this section.

https://www.st.com/resource/en/reference_manual/dm00031020.pdf

This topic has been closed for replies.

1 reply

ST Technical Moderator
October 29, 2019

Hello @TDK​ ,

You are right, we will correct this error for all impacted STM32F4 and STM32F2 reference manuals .

Thanks for bringing this to our attention.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks