Error instantiating RTE components Error #542: API '::Board Support.LED:1.0.0(API)' required by component 'Keil.STM32F4-Discovery::Board Support:LED:2.0.0' is missing
I'm using Windows 10 and arm KEIL IDE along with STM32F407G-DISCOVERY board. I'm a very beginner and trying to do something with LED. I'm stuck at the initial stage itself.
I have a problem with the LED API in the Board Support Package in the setup process. I tried to install two different DFPs using the Pack Installer ( latest version: 2.13.0 and little older version 2.11.0). But with both of them I see errors. Can someone please help
Error instantiating RTE components
Error #542: API '::Board Support.LED:1.0.0(API)' required by component 'Keil.STM32F4-Discovery::Board Support:LED:2.0.0' is missing