Skip to main content
Visitor II
October 10, 2024
Solved

Error in RM0490 Rev. 4 Section 6.2.6

Status bits in the RCC internal clock source calibration register (RCC_ICSCR) indicate which clock(s) is (are) ready and which clock is currently used as a system clock.

Should be the following:

Status bits in the RCC clock control register (RCC_CR) indicate which clock(s) is (are) ready.

Status bits in the RCC clock configuration register (RCC_CFGR) indicate which clock is currently used as a system clock.

This topic has been closed for replies.
Simon.T
Simon.TBest answer
ST Employee
October 10, 2024

Hello @MorganG ,

 

I confirm the issue, the link and the content will be changed. Thanks for spotting and reporting it. This will be fixed for the next document revision. 

 

Best regards,

 

Simon

2 replies

ST Technical Moderator
October 10, 2024

Hello @MorganG and welcome to the Community,

Thank you for raising this issue.

I will check this and will get back to you soon with update (Internal ticket is submitted ID 193408 - not available outside of ST)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Simon.T
Simon.TBest answer
ST Employee
October 10, 2024

Hello @MorganG ,

 

I confirm the issue, the link and the content will be changed. Thanks for spotting and reporting it. This will be fixed for the next document revision. 

 

Best regards,

 

Simon