Skip to main content
TKrop
Associate II
Oct 15, 2019 7:28 PM UTC
Solved

Error in RM0440 Rev 1 and 2

On page 92, table 7 contains flash memory addresses and their sizes.

For every address range, the difference between the start and end address is 0x7FF, i.e. 2 KiB.

However, for Page 127 in both Bank 1 and Bank 2, the range is listed to be 0xFFF, i.e. 4 KiB.

The error here is that both starting addresses should end with '800' instead of '000'.

Additionally, table 8 is missing a hyphen on its Page 127 address range.

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Oct 21, 2019 1:29 PM UTC

Hello,

You are right, this should be corrected: Page 127 range in Table7 is:

0x0803 F800 - 0x0803 FFFF.

0x0807 F800 - 0x0807 FFFF.

We will correct this in the next RM0440 release.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

1 reply

Imen.DBest answer
ST Technical Moderator
Oct 21, 2019 1:29 PM UTC

Hello,

You are right, this should be corrected: Page 127 range in Table7 is:

0x0803 F800 - 0x0803 FFFF.

0x0807 F800 - 0x0807 FFFF.

We will correct this in the next RM0440 release.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks