Skip to main content
Nikita91
Lead II
April 11, 2022
Solved

Error in RM0432 Rev 9 for MCOSEL[3:0]: Microcontroller clock output ? EDIT: Sorry, no error in the manual.

In the manual P 263:

Bits 27:24 MCOSEL[3:0]: Microcontroller clock output
Set and cleared by software.
0000: MCO output disabled, no clock on MCO
0001: SYSCLK system clock selected
0010: MSI clock selected.
0011: HSI16 clock selected.
0100: HSE clock selected
0101: Main PLL clock selected
0110: LSI clock selected
0111: LSE clock selected
1000: Internal HSI48 clock selected

But the real order is

0000: MCO output disabled, no clock on MCO
0001: LSE clock selected
0010: LSI clock selected
0011: HSE clock selected
0100: HSI16 clock selected.
0101: Main PLL clock selected
0110: SYSCLK system clock selected
0111: MSI clock selected.
1000: HSI48 clock selected

This is the order in the CubeMX mux setting for the MCO output.

This topic has been closed for replies.
Nikita91
Nikita91Best answer
Lead II
April 11, 2022

Sorry...

I misread my own code from a few years ago.

There is no error in the manual.

6 replies

waclawek.jan
Super User
April 11, 2022
Nikita91
Nikita91Author
Lead II
April 11, 2022

I'm only saying that the order in CubeMX matches what I observe on pin PA8.

When I put 1 in the RCC->CFGR / RCC_CFGR_MCOSEL field, I get a frequency of 32768 and not 120MHz.

I think the people who wrote the HAL followed the RM, the people who did MX followed the hardware specification.

waclawek.jan
Super User
April 11, 2022

> When I put 1 in the RCC->CFGR / RCC_CFGR_MCOSEL field, I get a frequency of 32768 and not 120MHz.

That sounds convincing indeed.

I would like to confirm, but don't have an 'L4+ at hand... :(

JW

Piranha
Principal III
April 11, 2022

If this is true, it could be the same for L4 series. I'll test it on L432 and report.

Nikita91
Nikita91AuthorBest answer
Lead II
April 11, 2022

Sorry...

I misread my own code from a few years ago.

There is no error in the manual.

waclawek.jan
Super User
April 11, 2022

Thanks for coming back with the solution.

You may perhaps select your post as Best so that thread is marked as solved.

JW