Question
Error in RM0368 Reference Manual SPI Register Map or I miss something ?
Hello,
I am working with STM32F401RE and I spotted something strange about the SPI Register map (Reference manual RM0368 Rev 5,Table 9.3, p611).
9 registers are described in the SPI chapter, but only 8 are include on the SPI Register Map, it is missing the SPI_CR2 register.
Offsets and addresses are ok and there is no serious risk of error, but I don't know if it's normal and I didn't understand why this register is not in the register map or if it's a mistake.
Any explaination will be welcome ! :)