Skip to main content
Moritz1
Associate III
March 13, 2023
Solved

Error in reference manual of STM32G4

I think there is an error in the reference manual (RM0440 Rev 7) in chapter 24.5 - COMP interrupts.

At the end of this chapter it says: "Interrupt events are flagged through COMP_CxCSR flags."

But in COMP_CxCSR register there is no flag for interrupt event?

The Interrupt is handled by EXTI, so the Flags are in the EXTI_PR1/EXTI_PR2 register.

Or do I miss something?

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
March 15, 2023

You are welcome :)

I confirm the error. An internal ticket (ID 147682) is submitted to correct the sentence which should be:  

0693W00000aJ3AkQAK.png(PS: ID 147682 is an internal tracking number and is not accessible or usable by customers).

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

4 replies

waclawek.jan
Super User
March 14, 2023

This is probably one of those not-that-well-thought-through half-truth we see ocassionally in the RMs, maybe in response to some customer's complaint. I went through almost all other STM32 RMs and never seen this particular line. Most of them at the end of COMP interrupts subchapter contain a table - a not very useful either - such as this for 'U5:

0693W00000aItd8QAC.pngWhat the "...flagged through..." in 'G4 RM is supposed to mean is, IMO, the "Event flag" column.

@Imen DAHMEN​ , can this sentence in 'G4 RM please be removed or at least rephrased to be less confusing? Or, maybe it would be the best to bring it in line with other STM32 RMs, adding this table (and then also consider adding it to 'F3xx RMs, too).

Thanks,

JW

ST Technical Moderator
March 15, 2023

Hello,

@Community member​, thank you for pointing out this post.

 I am checking it and take the necessary actions.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
waclawek.jan
Super User
March 15, 2023

Thanks, Imen.

Jan

Imen.DBest answer
ST Technical Moderator
March 15, 2023

You are welcome :)

I confirm the error. An internal ticket (ID 147682) is submitted to correct the sentence which should be:  

0693W00000aJ3AkQAK.png(PS: ID 147682 is an internal tracking number and is not accessible or usable by customers).

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks