Skip to main content
AdoringLamb
Associate
Apr 27, 2025 1:46 PM UTC
Solved

Error in initializing ST-LINK device in all boards

i have been using stlink v2 for a while now, but today it wouldn't connect with any of my stm32 boards the error mesage that apears is 

STMicroelectronics ST-LINK GDB server. Version 7.9.0

Copyright (c) 2024, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Target no device found

 

Error in initializing ST-LINK device.

Reason: No device found on target.

 

i have no clue what it could be, i tried in two different pcs with stm32 cube ide in the 1.17 and 1.18 version, i have tried updating the stlink software in the cube ide , in the programmer and in the st link utility, nothing is really working, the boards are fine cause i can connect them to the st programmer using usb.

Need help, Thanks

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
Apr 27, 2025 5:52 PM UTC

...

>What it shows on CubeProgrammer, if you only wire pin19 to pin 1 or 2 ?

 

+

What you connected, when used last time ? 5V ?

If you feel a post has answered your question, please click on " Best Answer ".

21 replies

AScha.3
Super User
Apr 27, 2025 2:14 PM UTC

Is it genuine STM or V2 "stick" ?

Connect with CubeProgrammer and show, what its telling.

 

If you feel a post has answered your question, please click on " Best Answer ".
AdoringLamb
Associate
Apr 27, 2025 2:17 PM UTC

AdoringLamb_1-1745763390684.png

its a genuine stlink v2 

AScha.3
Super User
Apr 27, 2025 2:19 PM UTC

Ooo.. target : 0,52V - that cannot work !

power your target to 3v3 and try again. (or you forgot to connect the vcc sense to st-link ?)

If you feel a post has answered your question, please click on " Best Answer ".
AdoringLamb
Associate
Apr 27, 2025 2:36 PM UTC

thats weird cause its 3.3 v in the input

AdoringLamb_3-1745764551239.png