Skip to main content
Associate II
November 18, 2025
Question

Error in initializing ST-LINK device

Hello everyone i had today while working with the NUCLEO H753ZI board and when i try to upload the code i had faced this error message when i try to connect with the cube programmer i faced this error and my LD6 pin is glowing with low intensity can you please tell me why i facing this issue whethere this could be any short problem or anything else

Screenshot (5).png

 

WhatsApp Image 2025-11-18 at 8.00.21 PM.jpeg

5 replies

TDK
November 18, 2025
"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
November 18, 2025

Or:

 

UM2407 says LD6 glows lit when an overcurrent happens (7.4.1 Power supply from ST-Link-V3E USB connector).

Do you consume too much power somewhere?

 

It is hard to tell from the 2nd pic. Is JP2 1-2 (STLINK) closed?

Associate II
November 19, 2025

@mfgkw Yes it is closed sir. I haven't connected the any external device which condumes more power i have been checking the interupt pins with the weigamd readers.