Skip to main content
Senior
Jul 6, 2024 5:44 AM UTC
Solved

Error in Final Launch Sequence

I am trying to upload the code to my target STM32F407 but below error is showing up. I tried some of suggestions but problem is still there. I am using Version: 1.15.1.   Debug log file also attached. 

1) Doing Mass Erase of flash,

2) Updating ST Link Firmware

3) Set Reset Behavior: None

4) Uncheck Enable Live Expressions

Nico3_0-1720244408387.png

 

Update:   I moved to STM32Cube programmer instead of using STM32cubeide, and able to upload the code after reducing ST-Link Frequency to 15Khz. Is it due to my target board poor design or something else. I am using Discovery Board ST-LINK to upload

 

 

 

 

This topic has been closed for replies.
Nico3Best answer
Senior
Jul 7, 2024 6:10 AM UTC

 Pls note issue has been solved. The problem was with jumper cables between ST-LINK and Target board. We used new cables and all in single ribbon, so now it is working fine.  

I conclude EMI was issue..

3 replies

Nico3AuthorBest answer
Senior
Jul 7, 2024 6:10 AM UTC

 Pls note issue has been solved. The problem was with jumper cables between ST-LINK and Target board. We used new cables and all in single ribbon, so now it is working fine.  

I conclude EMI was issue..

Visitor II
Apr 16, 2025 9:40 AM UTC

i downloaded and installed STM32 ST-LINK Utility. Then I erase chip by STM32 ST-LINK Utility. Then I open program in Stm32Cube and run program with stm32 board. It works. 

Andrew Neil
Super User
Apr 16, 2025 9:46 AM UTC

@chau  Note that the old ST-Link Utility is long obsolete - although it may still work with older parts (like the F407 here), it's not going to help for newer ones.

As the OP said, STM32CubeProgrammer is the way forward.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.