Question
Error Flash download failed - ''Cortex M4''
Posted on July 18, 2014 at 12:14
Hello,
I´m doing my bachelor thesis at the moment by designing a hardware with a microcontroller. I´m using a self made board with the STM32F407ZG microcontroller. My board has a JTAG adapter for programming. All the other components which are required for reset an so on are placed in the same way like on the STM32F4 Eval board of ST. I´m using keil uvision 5 and a Ulink2 adapter. After I finished my board I tryed to flash it with a programm which is working on an eval-board, but it just worked the first time I tryed it with no errors. Since then I can´t operate anytime with my board. If I try to flash it always brings a timeout error.which says ''Flash timeout. Reset the target and try it again''. So my question is if there is a way to set the microcontroller back to the factory settings, by an external setup. thanks for any help