Error! Failed to read target status
Hello everyone, I am trying to run a program on my board. I could use the same method to debug the program on a different chip but now it is not working on this board. I am using the st-link v2 programmer. but I get this error:
******************************************************************************
STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61235
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
Log output file: C:\Users\BMANOU~1\AppData\Local\Temp\STM32CubeProgrammer_a10724.log
ST-LINK SN : 56FF6D064883535246222487
ST-LINK FW : V2J34S7
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x448
Device name : STM32F07x
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M0
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a10724.srec
File : ST-LINK_GDB_server_a10724.srec
Size : 49964 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 24]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:02.525
Verifying ...
Download verified successfully
Error! Failed to read target status
Debugger connection lost.
Shutting down...
******************************************************************************
Any help is appreciated. Thanks