Skip to main content
mathijs
Visitor II
Feb 12, 2015 10:19 AM UTC
Question

Error assert_param

Posted on February 12, 2015 at 11:19

Hi

I have a problem generating a I2C-code for my STM32F2xx.

I used the STD_PERIPH_DRIVER and the files it contains. 

When i compile, i get an error like this: 

Error[Li005]: no definition for ''assert_param'' [referenced from C:\Users\user\Dropbox\School\Masterproef\Project\I2C-test\Debug\Obj\stm32f2xx_i2c.o] 

Is there anyone who can help me? Assert_param occurs in a lot of files. 

I guess i just miss the file that defines the function.

Greetings
    This topic has been closed for replies.

    1 reply

    AvaTar
    Senior III
    Feb 12, 2015 11:34 AM UTC
    Posted on February 12, 2015 at 12:34

    You need to add the define ''

    USE_STDPERIPH_DRIVER

    '' somewhere to your build settings. How you do it depends on your build environment. In case of a makefile, add ''

    -DUSE_STDPERIPH_DRIVER

    ''.

    The ''

    assert_param()

    '' macros is defined in the

    stm32xxx_conf.h

    file, which gets included from the

    stm32fxxx.h

    file - but only if

    USE_STDPERIPH_DRIVER

    is defined.

    (Just assuming the F2xx stdperiph library is designed the same way as those for F0, F1, F3 and F4 ...).