Question
Errata Sheet Es0291 error for STM32F070xB
Posted on September 23, 2016 at 08:26
en.DM00148061.pdf 1.2.2 says:
USART4_RX does not work as output on PC11 As a consequence, single wire half duplex mode is not supported with pin PC11. ->Use USART4_RX mapped on PA0 instead on PC11 (PA0 is USART4_TX!!) actually PC10 (TX) is used for single wire half duplex mode (without pin swapping: don't know if this even works, cannot be selected for single wire mode in CUBE) PA0 is also TX. Big question: does PC10 actually work for single wire half duplex mode as USART4? could anybody shed a little light into this confusion? #singlewire-usart4-mode