Skip to main content
Timm Knape
Visitor II
May 30, 2018
Question

Errata for AN3155

  • May 30, 2018
  • 0 replies
  • 750 views
Posted on May 30, 2018 at 11:27

Hi,

sorry, if this forum is the wrong place, but I did not find a better one :)

In AN3155 (USART protocol used in the STM32 bootloader; DocID17066 Rev 7) on page 7 it is written:

2. for each command the host sends a byte and its complement (XOR = 0x00)

but if I XOR a byte and its complement I get 0xff as result, not 0x00.

I guess the correct meaning is restored if the XOR part is removed completely on checksums over a single byte. This also happens in byte 9 of the Read Memory Command (here the XOR should be replaced by complement). I do not know if any other documents are affected.

Sadly there is no contact in this document to address the problem directly.

Kind regards,

Timm.

    This topic has been closed for replies.