Skip to main content
Shadow
Associate II
September 6, 2022
Solved

Erasing a Flash Page of STM32L4R5 doesn’t work

I'm trying to erase a Flash Page of from my firmware Application with STM32L4R5 using the function 'HAL_FLASHEx_Erase()'. The Application Presence Key is stored in this page. It needs to be erased by the Application to activate the Bootloader (this is not the internal Bootloader) in Firmware Update mode.

The test code is copied below. It works properly if it is in the main() function of the Bootloader. However, erasing the page fails if the code is in the main function of the Application. The function returns ‘HAL_ERROR’ and the flashStatus is not 0xFFFFFFFF as it should be.

Does anybody know if I’m missing something here?

FLASH_EraseInitTypeDef EraseInitStruct; // Flash Page Erase Structure
uint32_t flshStatus = 0; // Flash Page Erase Status
 
// Flash Erase Structure Init
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Banks = FLASH_BANK_2; // Bank 2
EraseInitStruct.Page = 255; // Last Flash Page
EraseInitStruct.NbPages = 1; // One Page
 
// Unlock FLASH Control Register
HAL_FLASH_Unlock();
 
// Clear OPTVERR Bit Set on Virgin Samples
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
 
// Erase Specified Flash Page
uint32_t retStat = HAL_FLASHEx_Erase(&EraseInitStruct, &flshStatus);
 
// Lock FLASH Control Register
HAL_FLASH_Lock()

This topic has been closed for replies.
Shadow
ShadowBest answer
Associate II
December 2, 2022

Hi,

Unlocking the flash wasn't the issue. The solution was clearing two more flags:

// Unlock FLASH Control Register

  HAL_FLASH_Unlock();

  // Clear Bits Set on Virgin Samples

  __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);

  __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_PGSERR);

  __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_PGAERR);

  // Erase Specified Flash Page

  HAL_FLASHEx_Erase(&EraseInitStruct, &flashStatus);

  // Lock FLASH Control Register

  HAL_FLASH_Lock();

Thanks!

2 replies

ST Technical Moderator
December 2, 2022

Hello @Shadow​ 

Try Unlock the flash before the init of structure to erase.

I understand that the function of erased is not yet called but Unlocking Flash mechanism may need the whole structure to be set before. It is like it could be overriden after that.

After try to write some words and read it back. So that you won't leave it empty after locking.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Shadow
ShadowAuthorBest answer
Associate II
December 2, 2022

Hi,

Unlocking the flash wasn't the issue. The solution was clearing two more flags:

// Unlock FLASH Control Register

  HAL_FLASH_Unlock();

  // Clear Bits Set on Virgin Samples

  __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);

  __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_PGSERR);

  __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_PGAERR);

  // Erase Specified Flash Page

  HAL_FLASHEx_Erase(&EraseInitStruct, &flashStatus);

  // Lock FLASH Control Register

  HAL_FLASH_Lock();

Thanks!