Question
Erase FW + Download FW from SD-Card
Posted on August 03, 2013 at 13:42
Hello ,
I have a more theoretical question ( for now ) , suppose i want to update the firmware on the STM32 , lets say i put the new FW file on the SD-card , the current FW should detect it and do the update . How can i do this ? should i define a protected section on the flash (where the code is located) and defined it as a ''boot-loader'' section where i will have the limited abilities to read from SD-card and write the new FW to the firmware sector on the ''flash'' ? If this is true , i should modify my start-up script to jump first to the boot loader function main , and not to the firmware main , and if there is no update available i should jump to the firmware main, correct?