Skip to main content
4lch
Associate II
Nov 29, 2024 7:51 PM UTC
Solved

Ensure a pin is low while in bootloader

Hi and thanks in advance !

My application uses a STM32G0B0 to control an LED driver through PWM among other things (pin (26)-PB14).

The device can receive commands and I have added an option to jump to bootloader through a special command to perform firmware updates through USB. This works well, however, the pin I use to control the PWM LED driver remains high while in the bootloader, which could cause the LED board to heat up too much.

I have tried to stop the timer and configure the pin low before jumping, and it works to pull the pin low right until the jump is actually made.

A pull-down resistor soldered between the PWM pin and GND did not change this behaviour either.

Could the bootloader be forcing this specific high ? What other options could there be to make sure it remains low while in the bootloader ?

Here is the current bootloader jump code, stripped of my attempts to turn off the pin before jumping :

 

 

void JumpToBootLoader() {

	void (*SysMemBootJump)(void);

	HAL_DeInit();

	/* Disable all interrupts */
	__disable_irq();

	/* Disable Systick timer */
	SysTick->CTRL = 0;

	/* Set the clock to the default state */
	HAL_RCC_DeInit();

	/* Clear Interrupt Enable Register & Interrupt Pending Register */
	for (uint32_t i=0;i<sizeof(NVIC->ICER);i++)
	{
		NVIC->ICER[i]=0xFFFFFFFF;
		NVIC->ICPR[i]=0xFFFFFFFF;
	}

	/* Re-enable all interrupts */
	__enable_irq();

	/* /!\ THIS LINE IS REQUIRED TO REMAP MEMORY BY HAND BEFORE JUMPING /!\ */
	SYSCFG->CFGR1 = 0x01;

	SysMemBootJump = (void (*)(void))(*((uint32_t *)(0x1FFF0000 + 4)));
	__set_MSP(*(__IO uint32_t *)0x1FFF0000);

	SysMemBootJump();
}

 

 

Thanks in advance !

This topic has been closed for replies.
gbm
gbmBest answer
Super User
Nov 30, 2024 6:33 AM UTC

The default pin configuration for every STM32 is specified in RefMan - GPIO - Registers; see the reset values of MODER and PUPDR. One important thing which is not explicitly mentioned in this section of RefMan is the default behavior of CC and DBCC pins in MCUs equipped with UCPD peripheral (like G0B). To keep it short: all the CC pins may have 5k1 pulldowns active after reset, but this does not interfere with your app.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

8 replies

gbm
Super User
Nov 29, 2024 8:04 PM UTC

The explanation of boot mode behavior may be found in AN2606. Please Read The Fine Document.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
4lch
4lchAuthor
Associate II
Nov 29, 2024 11:55 PM UTC

Thanks a lot for pointing me to this document !

Indeed it mentions that the pin is used as SPI2 MISO in push-pull, pull-down mode, but set to 3.3V "on the bootloader start-up after SPI initialization as soon as the bit DMATx enable on SPI CR2 register is set to 0x1"

Seems like dead-end with this current pin, I will look into moving it to another one that is not used during the bootloader. I assume that pins not used specifically during the bootloader should be floating or hopefully weak enough that an external pull-down resistor should guarantee that it is low ?

Thanks again !

gbm
gbmBest answer
Super User
Nov 30, 2024 6:33 AM UTC

The default pin configuration for every STM32 is specified in RefMan - GPIO - Registers; see the reset values of MODER and PUPDR. One important thing which is not explicitly mentioned in this section of RefMan is the default behavior of CC and DBCC pins in MCUs equipped with UCPD peripheral (like G0B). To keep it short: all the CC pins may have 5k1 pulldowns active after reset, but this does not interfere with your app.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
waclawek.jan
Super User
Nov 30, 2024 10:32 AM UTC

In many cases, it's better to write your own bootloader over which you have full control, rather than trying to work around the peculiarities (not always well documented) of the default one.

JW

4lch
4lchAuthor
Associate II
Nov 30, 2024 11:29 AM UTC

Thanks a lot, this is not an option I had in mind !  I will look into that. I only need to setup USB DFU for firmware updates during the bootloader so hopefully it should not be too bad !