Skip to main content
franco2
Associate II
October 22, 2007
Question

energy meter STM32F101xx

  • October 22, 2007
  • 6 replies
  • 1181 views
Posted on October 22, 2007 at 12:31

energy meter STM32F101xx

    This topic has been closed for replies.

    6 replies

    franco2
    franco2Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    He at All

    Sorry for my continualy question

    The my application must be function in battery mode in this function what is the current used when the processor is in standby mode? is 2uA is correct? plus if the RCT is on is 1.4uA tot. the current is 3.4uA?

    The time from standby to a main function is 50us?

    Thanks

    Franco

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Hi Franco,

    What is your battery voltage ; is it 3.0v or less /more ?

    You can refer to our Datasheet on web (rev3) it includes all what you need

    and also you can have a look on our Low power reference for your energy meter design with STM32 in this Application Note

    http://www.st.com/stonline/products/literature/an/13922.pdf

    : ''STM32F101xx and STM32F103xx low-power modes''. Enjoy ;)

    Regards, STOne-32

    obtronix
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    looking at the new datasheets the startup time is 150usec + 200 usec if you are using the PLL.

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Hi obtronix,

    150 and 200 µs are the Maximum timing in worst cases condition ( Hot /Cold temperatures, low/High VDD level from 2 to 3.6Volts.

    The typical value is of course less , for example only 50µs for Wake-up from standby mode + your reset firmware code & PLL lock time etc....

    By the way, what is your application configuration and your expected life of Battery ? are you using other components such as a Glass LCD like on most of metering products.

    Regards, STOne-32

    [ This message was edited by: STOne-32 on 21-10-2007 19:38 ]

    franco2
    franco2Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Thanks for your assistance

    Franco

    obtronix
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Quote:

    On 21-10-2007 at 19:37, Anonymous wrote:

    Hi obtronix,

    By the way, what is your application configuration and your expected life of Battery ? are you using other components such as a Glass LCD like on most of metering products.

    Regards, STOne-32

    I am using a glass LCD, which brings up a question, do you think the STM32 series will ever have a internal LCD driver like the MSP430/AVR/MaxQ chips have? Seem like a common thing required for power meters/glocose meters, which this processor is aimed at (according to ST's brochures). Takes a lot of area to add an external LCD driver chip.

    [ This message was edited by: obtronix on 23-10-2007 03:36 ]