Skip to main content
Associate III
November 5, 2024
Question

"ELF/DWARF Error: Unknown" and "Failed to load debugee" errors in IAR

Hi, 

I'm working on a project where I have added x-cube STL for self testing, I'm using IAR 9.30.1 and STM32H745ZIT3

Unable to debug or load the code into my target, why this post build command causing problem or CRC injecting in that particular area 0x080FF000 

 

Suggest me any method or how to troubleshoot this error in setting or options of IAR tool

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
November 5, 2024

Well you can't plant CRC's mid-image, or in a manner that corrupts the object file.

Normally one would quantify the size of the sections, as built, and append checksums, CRC or signing. Some cases you'd need to expand sections to allow for this.

Perhaps inspect via objdump, objcopy, fromelf or similar inspection tools, and try to understand what you're breaking.

Perhaps write your own code to manage this? The ELF format is pretty well documented, and we're SW engineers, right?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Lucifer37Author
Associate III
November 5, 2024

But it's part of X-Cube STL package, Integrating static library STL_Lib_cm7.a and in post build must use this command 

STM32_Programmer_CLI.exe -sl "$PROJ_DIR$/CM7/Exe/source_code.out" 0x08000000 0x08100000 0x400

So I'm saying the STM CUBE programmer to put CRC in particular that area, It automatically does....

So what changes I need to do in linker script or loader, adjust any addresses