Skip to main content
Greusard Alexandre_2
Associate II
Oct 9, 2017 4:23 PM UTC
Question

Eclipse/workspace configuration for custom boards

Posted on October 09, 2017 at 18:23

Hello everyone!

I'm new in the stm32 world and I have to say, I realy like it!

I am under Ubuntu and I use '

Eclipse System Workbench

' pre-configured IDE. I only use standart-stm32 library for now.

I had some practise on a stm32f0-discovery board (no problem here), but now I have to work on a

stm32f107vc UC on a custom board

. When I created my new project(on eclipse system workbench), I also created a new board with the appropriate UC.
  • My first problem (and workaround): Interruptions made my code stop , workaround -> I modified the file 'startup_stm32.s' and added Interruptions to my vector table 'g_pfnVectors', it works for now.
  • My second problem:

    USART TX sending bad characters:

    When I send 'Hello\r\n' through USART, I read 'ZE]F�' on the TX. But if I make a new project, selecting a NUCLEO stm32F103 board, and I use exactly the same code to program my stm32f107 board, it works....

So my question would be:

How to configure my project in the case of a Custom board (considering I am working with eclipse IDE, or not)?

I would be very thankfull if anyone could give me any idea, or track to follow... and I hope my question is clear enough.

Alex

#stm32 #eclipse #custom-board #configuration
    This topic has been closed for replies.

    4 replies

    waclawek.jan
    Super User
    Oct 9, 2017 5:26 PM UTC
    Posted on October 09, 2017 at 19:26

    Misconfigured system clock?

    JW

    Greusard Alexandre_2
    Associate II
    Oct 10, 2017 2:19 PM UTC
    Posted on October 10, 2017 at 14:19

    Thanks for the answer. Well I don't think it is, as I said, the exact same code will work on an other board description.

    I found an other workaround, I changed a preprocessor option of my compiler from 'STM32F10X_CL' to 'STM32F10X_MD' and now I receive the good characters from the stm32.

    The strange thing is that I am working on a stm32f107 µC, wich is a 

    Connectivity line device

    so it should work with the 'STM32F10X_CL' option.

    I dont understand whats going on...

    If someone has an idea, it would be very appreciated!!

    waclawek.jan
    Super User
    Oct 10, 2017 3:09 PM UTC
    Posted on October 10, 2017 at 15:09

    the exact same code will work on an other board description.

    Only if it would be the same *binary* would it deserve the 'exact same code' label. I doubt this is the case.

    So show us how do you set the system clock, or check it through outputting to MCO and measuring it.

    In fact it's the APB setting not the system clock as such, so you might also investigate that.

    JW