Question
Eclipse and CodeSourcery ARM Sourcery G++ question
Posted on October 22, 2011 at 02:19
Hi
I have eclipse 3.6 with GNU ARM C/C++ development support configured.However, it can generate hex file with warning: cannot find entry symbol Reset_Handler; defaulting to 08000000. Not sure will this effect the hex file.So I download it to F4discovery board with STM32 ST-LINK utility, reset the board, the program can not run. And I program it with hex that from demo project of the board and it works.The codes I wrote can work in atollic's truestudio.I convert them to bin file with post-build command.their size are totally different, it is sure that compile from eclipse has problemTwo files are attachedSo I wander that is it due to my C/C++ build configuration errors or something else?Is there any configure tutorial for cortex m4?This one works for Cortex M3, but GNU ARM plugin is easier to use.Thanks