Question
Easiest way to get data out of STM32F0308-DISCO?
Posted on July 13, 2016 at 23:21
So, the Cortex-M0 doesn't support tracing (so it doesn't support semihosting).
The board has a TX & RX pin and a corresponding pair of solder bridges, but the manual says ''reserved''. So is it best to connect an external USB->3v3 Serial to UART1 and do that or is there a way I can use the TX/RX on the board? #stm32f0308-disco-stm32f0