Question
Early waking Up from STOP mode
Dear,
I use SM32L152, I go to STOP mode regularly and as the possible source of waking up is either RTC or External interrupt. It works Fine until I change the System clocks from MSI 4 MHz to for example HSI on 16 MHz. If I change it, then MY MCU is woken up even if RTC alarm has not expire yet and no external interrupt happened.
I am really desperate. I will appreciate every advice.
Thank you very much, Jan.