Skip to main content
Harish1
Associate III
Jul 4, 2022 1:23 PM UTC
Solved

Dynamic exception priority change in STM32 Cortex-M4

I am using the timer interrupt and currently, it has priority 3 once I get into the ISR then I want to change the priority to 2. I have used like below but the priority not changing.

NVIC->IPR[6] |= NVIC_IPR6_PRI_25 & 0x22222222;

__dsb(0);

In above, __dsb(0) or __dsb(1) I am not getting?

I am using the Keil environment.

    This topic has been closed for replies.
    Harish1
    Harish1Best answer
    Associate III
    Jul 5, 2022 7:06 AM UTC

    I made a small mistake that's why it is not working and it is working now.

    Thank you all.

    7 replies

    gbm
    Super User
    Jul 4, 2022 1:29 PM UTC
    1. Don't do it. I'm 99% sure you don't need to change the priority.
    2. Use NVIC_SetPriority() to change the priority. This should be done while the interrupt is disabled and not during its service.
    My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
    Harish1
    Harish1Author
    Associate III
    Jul 4, 2022 4:29 PM UTC

    But if the cortex m4 supports the dynamic exception priority change then why you are not suggesting implementing it?

    I have already set the priority levels before ISR run but I want to make the nested to reach my goal as explained in the below anwere.

    Tesla DeLorean
    Guru
    Jul 4, 2022 1:36 PM UTC

    Which STM32 part are we talking about?

    What are the values in NVIC->IPR[6] before/after this operation?

    Are there better ways of approaching the end goal?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Harish1
    Harish1Author
    Associate III
    Jul 4, 2022 4:27 PM UTC

    I am using STM32L475.

    The existing priority is configured as NVIC->IPR[6] = 0x00003300 but I want to change this priority to 0x00002200 during ISR to get the nested interrupt functionality.

    The main goal is here that implements the nested interrupt for the timer interrupt.

    0693W00000QKP3JQAX.pngIn the above figure, the timer counter goes into up-down mode and an interrupt generates for every counter equal to zero. When the 1st interrupt comes the function starts at T = 0 and ends at T=x as the size of the function is too large. If I don't use the 2nd interrupt, the functionality gets disturbed. And I want to update the comparator values in the 2nd interrupt that's it and I will return to the 1st interrupt and this will go to main.

    0693W00000QKP3xQAH.png 

    As the interrupt is the same and as per NVIC the 1st interrupt completes and then only goes to 2n interrupt because of the same priority. I want to make the 2nd interrupt priority as 2 so that this has the highest priority and nested action come.

    Pavel A.
    Jul 4, 2022 6:11 PM UTC

    There is a better way to do this, not using "gray zone" tricks.

    When the 1st interrupt occurs, immediately trigger a software interrupt with lesser priority and return from the interrupt. From the ISR of the software interrupt call the "huge function". When the 2nd interrupt occurs, it will naturally preempt the "huge function".

    ​

    ​

    Harish1
    Harish1AuthorBest answer
    Associate III
    Jul 5, 2022 7:06 AM UTC

    I made a small mistake that's why it is not working and it is working now.

    Thank you all.