Skip to main content
DiBosco
Senior
May 20, 2021
Question

Dual Bank Memory Variants

  • May 20, 2021
  • 2 replies
  • 581 views

Folks,

When you have a dual bank STM32, at run time, is it just one contiguous area of memory. So, for example, if you were running out of the top of bank 1 and the next instruction was in bank 2, would the program seamlessly just jump from running out of bank 1 to bank 2?

Thanks!

    This topic has been closed for replies.

    2 replies

    Uwe Bonnes
    Chief
    May 20, 2021

    On the flash-castrated devices, behaviour is device and option -byte dependant. Carefulle study the reference manual and try to understand the options.

    DiBosco
    DiBoscoAuthor
    Senior
    May 20, 2021

    Flash-castrated? Sorry to be slow, but what does that mean?