Question
drop in replacement for STM32L433.
Hi
I am using a STM32L433 100 pin and require more memory as using a display. I have looked at the STM32L452VET6 100pin , and looks identical apart from having more memory. I only use the HAL for initialisation and USB interface. Looking at the HAL files it says for the STM32L4xx, does this mean the same files can be used? And all I have to do is change the memory size in the linker file?
Best Regards
Scott