Skip to main content
sanjib
Associate III
July 31, 2014
Question

Driving PLL using internal oscillator in stm32f030

  • July 31, 2014
  • 2 replies
  • 612 views
Posted on July 31, 2014 at 11:41

The system clock of stm32f030c8t6 is 48 mhz ....I want to achieve the maximum frequency by using internal osc (8 Mhz) driving the PLL insread of external Osc. I was able to achieve with the help of external osc....How can I achieve using Internal osc (PLL(HSI)).

Please help
    This topic has been closed for replies.

    2 replies

    ivani
    Visitor II
    July 31, 2014
    Posted on July 31, 2014 at 15:59

    The PLL could use HSI/2 as input (PLLSRC = 0 in RCC_CFGR). Then you need to select PLLMUL=10 (PLL multiplier x12) in the same register.

    Tesla DeLorean
    Guru
    July 31, 2014
    Posted on July 31, 2014 at 18:25

    static void SetSysClock(void)
    {
    /* Enable Prefetch Buffer and set Flash Latency */
    FLASH->ACR = FLASH_ACR_PRFTBE | FLASH_ACR_LATENCY;
    /* HCLK = SYSCLK */
    RCC->CFGR |= (uint32_t)RCC_CFGR_HPRE_DIV1;
    /* PCLK = HCLK */
    RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE_DIV1;
    /* PLL configuration = HSI/2 * 12 = 48 MHz */
    RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_PLLSRC | RCC_CFGR_PLLXTPRE | RCC_CFGR_PLLMULL));
    RCC->CFGR |= (uint32_t)(RCC_CFGR_PLLSRC_HSI_Div2 | RCC_CFGR_PLLMULL12);
    /* Enable PLL */
    RCC->CR |= RCC_CR_PLLON;
    /* Wait till PLL is ready */
    while((RCC->CR & RCC_CR_PLLRDY) == 0)
    {
    }
    /* Select PLL as system clock source */
    RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_SW));
    RCC->CFGR |= (uint32_t)RCC_CFGR_SW_PLL;
    /* Wait till PLL is used as system clock source */
    while ((RCC->CFGR & (uint32_t)RCC_CFGR_SWS) != (uint32_t)RCC_CFGR_SWS_PLL)
    {
    }
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..