Skip to main content
bradpitt119
Associate
Aug 29, 2012 7:23 PM UTC
Question

driver not found for STM32F4 Discovery board when I connect it to my pc

Posted on August 29, 2012 at 21:23

I have some similar problem with my new STM32F4 Discovery board. Neither my xp macine nor my windows 7 machine can recognize the board. The led lights are able to blinking. But the device driver is not able to install, the device is showing unknown in the device management.

I wonder if there is any technical support from STMicroelectronics.

Do I need to download some driver to install it manually from your website? Because I don't see any CD comes with the board.

Thanks.
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    Aug 29, 2012 9:08 PM UTC
    Posted on August 29, 2012 at 23:08

    ST-LINK Utilities and Drivers

    http://www.st.com/jp/com/SOFTWARE_RESOURCES/TOOL/DEVICE_PROGRAMMER/stm32_st-link_utility.zip

    http://www.st.com/jp/com/SOFTWARE_RESOURCES/SW_COMPONENT/SW_DRIVER/st-link_v2_usbdriver.zip

    Stuff is usually bundled in tools chains like Keil or IAR

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    bradpitt119
    Associate
    Sep 8, 2012 3:02 AM UTC
    Posted on September 08, 2012 at 05:02

    I have tried both, even I also tried to install the driver from IAR.

    But it is still unknown.

    I am also having problem download and debug STM32F4 discovery in IAR. I got the attached errors. I guess may be these two problems are related.

    ________________

    Attachments :

    stm32f4_st_link.doc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I02T&d=%2Fa%2F0X0000000bSb%2FmG7xPwmi7_XgqYhee2VNizTeN8QP._DRbEL7WAUOsy8&asPdf=false
    bradpitt119
    Associate
    Sep 8, 2012 2:13 PM UTC
    Posted on September 08, 2012 at 16:13

    The driver works well with my xp machine. 

    So this is a computer specific problem. It got to be something with my acer window 7 machine.

    This computer has some problem to recognize new hardware. Some time ago I needed to delete the lower fillter or upper filter (I forget which one) to install a hardware.

    bradpitt119
    Associate
    Sep 8, 2012 2:28 PM UTC
    Posted on September 08, 2012 at 16:28

    finally I got it working, I have to cancel the driver searching from windows update when I insert the board.