Skip to main content
mikkel nielsen
Associate II
July 10, 2018
Question

download code to stm32f429

  • July 10, 2018
  • 5 replies
  • 1151 views
Posted on July 10, 2018 at 16:49

How to download the code to the microcontroller?

I am a beginner in stm32f429 and I don't understand that how to download the code to the microcontroller.

i am using eclipse(the IDE) on windows. i hope you can help because i am new a this

https://community.st.com/tags♯/?tags=quadrature%20encoder%20stm32f429

#stm32 #quadrature-encoder-stm32f429 #stm32f429
This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
July 10, 2018
Posted on July 10, 2018 at 21:13

On a truly 'Integrated' Development Environment you'd press a button and it would download and run/debug?

People usually download to the chip via a JTAG/SWD debug pod.

Is your STM32F429 on a Nucleo or Discovery board? Those have an on-board ST-LINK.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
mikkel nielsen
Associate II
July 12, 2018
Posted on July 12, 2018 at 08:38

It is a Discovery board i have 

Tesla DeLorean
Guru
July 12, 2018
Posted on July 12, 2018 at 09:11

You should be able to configure the debugger being used (ST-LINK via OpenOCD I'd presume, sorry using Keil here)

The alternate method to download .HEX and .BIN files is the ST-LINK Utilities.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AvaTar
Senior III
July 12, 2018
Posted on July 12, 2018 at 09:47

I would suggest to start with a free version of Keil uVision, IAR WB, or Atollic TrueStudio. They support the MCU and the discovery board out of the box, and you don't need to struggle with things like toolchain and debug pod integration.

Atollic is Eclipse based as well, and available for free since bought up by ST.

Battling with too many issues at once will only yield frustration.