Skip to main content
fernando maldonado_2
Visitor II
May 15, 2018
Question

Doubts about TAG within a new BSP PDSC file

  • May 15, 2018
  • 0 replies
  • 590 views
Posted on May 15, 2018 at 16:08

Hi Everyone!

   I'm developing a BSP file -board support package,  for a personal purpose card ' ad hoc ', using the STM32H753XI.

   While creating the PDSC file -pack description software component, I needed to include some TAGS <features> within TAG <board> threat.

   To take a secure reference, I used as a template the PDSC of the STM32H743I-EVAL, in its recent new version 2.1.0.

   There I found some <feature>, that perhaps I don't understand as correctly are like as how important are, after checking them all -in the reference file mentioned before STM32H743I-EVAL Datasheet.

   Then, through this post I'm sharing my doubts with st dot com Community, to know if some <feature> TAGS  within the reference PDSC file... are they really correct or needed.

      ... 

      ...

      <mountedDevice deviceIndex='0' Dvendor='STMicroelectronics:13' Dname='STM32H743XI'/>

      <compatibleDevice deviceIndex='0' Dvendor='STMicroelectronics:13' DsubFamily='STM32H743'/>

      <feature type='ODbg' n='1'     name='On-board ST-LINK/V2'/>

      <feature type='RAM' n='1'       name='8M x 32-bit SDRAM'/>

      <feature type='RAM' n='1'       name='1M x 16-bit SRAM'/>

      <feature type='ROM' n='1'      name='8M x 16-bit Nor Flash'/>

      <feature type='ROM' n='1'      name='512-Mbit Quad-SPI NOR Flash'/>

      Is it right? I think isn't complatible with the STM32H743I-EVAL Datasheet

      <feature type='USB' n='1'       name='High-Speed USB with micro-AB Connector'/>

      <feature type='USB' n='2'       name='Full-Speed USB with micro-AB Connector'/>

      <feature type='Joystick' n='1' name='5-position Joystick'/>

      <feature type='Camera' n='1'/>

      <feature type='Button' n='2'    name='Push-Buttons for Reset, Wakeup/Tamper or Key'/>

      <feature type='LED'                  n='4' name='4 color user LEDs'/>

      <feature type='GLCD' n='1' m='800.480' name='4-inch 800x480 TFT color LCD with capacitive touch panel'/>

     

 

Is it right? I think isn't complatible with the STM32H743I-EVAL Datasheet for the 5.7 inch TFT 640x480

      <feature type='Poti' n='1'         name='Analog Voltage Control for ADC Input (potentiometer)'/>

      <feature type='LineIn' n='1'     name='Audio CODEC with Stereo Line-In/Out and Speaker/Microphone'/>

      <feature type='LineOut' n='1'  name='Audio CODEC with Stereo Line-In/Out and Speaker/Microphone'/>

      <feature type='MIC'                  n='2' name='ST MEMS microphones'/>

      <feature type='Speaker'           n='2'/>

      <feature type='Other'               n='1' name='Digital Stereo Microphone'/>

      <feature type='CAN'                 n='1'/>

      <feature type='RS232'             n='1'/>

      <feature type='I2C' n='4'/>

      <feature type='ETH'                 n='1' name='10/100 Ethernet Port'/>

      <feature type='XTAL'               n='25000000'/>

      <feature type='PWR'               n='5' name='USB Powered'/>

      <feature type='PWR'               n='3' m='5' name='External Supply'/>

      <feature type='MemCard'        n='1' name='SDIO interface microSD card'/>

      <feature type='DIO' n='34' name='Motor Control Connector'/>

     

 

Is it right? I think isn't complatible with the STM32H743I-EVAL Datasheet

      <feature type='DIO' n='60' name='Daughterboard Extension header 1'/>

      <feature type='DIO' n='60' name='Daughterboard Extension header 2'/>

      <feature type='ConnOther' n='1' name='Motor control connector'/>

     

 

Is it right? I think isn't complatible with the STM32H743I-EVAL Datasheet

      <debugInterface adapter='ST-Link' connector='Mini-USB'/>

      <debugInterface adapter='JTAG/SW' connector='20 pin JTAG (0.1 inch connector)'/>

      <debugInterface adapter='JTAG/SW' connector='20-pin Cortex debug + ETM Trace (0.05 inch connector)'/>

</board>

   Community of st dot com, please, Can you help me with my doubts? Every kind of post will be welcome!

   fernando maldonado

   Argentina

    This topic has been closed for replies.