Skip to main content
bala_jss
Associate II
September 29, 2008
Question

Double memory in STM32F101v8T6?

  • September 29, 2008
  • 12 replies
  • 2078 views
Posted on September 29, 2008 at 19:20

Double memory in STM32F101v8T6?

    This topic has been closed for replies.

    12 replies

    bala_jss
    bala_jssAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:46

    Thank you STOne-32. When you say ''this RAM area is not ensured by ST to be functional '' , I really hope you mean RAM area between 10k and 20k and not the first 10K area!!

    Ride and IAR users, make sure you have the RAM configuration right !! This could be wrong on many of the chip variants.

    I have been using Ride, and this is how fixed it.

    Change the line ''RAMSize =20480'' to ''RAMSize =10240'' in STM32F101V8T6.sim file (in your ''....\Ride\Sim\ARM'' directory)

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:46

    Hi,

    Yes For sure ! I mean the extra RAM size from 10 to 20K is not functional , I guess all of you have understand this :)

    Cheers,

    STOne-32.