Skip to main content
SKosh.3
Associate
July 13, 2021
Question

Does the Wakeup from Standby work for 2 external events simultaneously in STM32L073 MCU?

Hi. I am using an STM32L073 based nucleo board. There are 2 external wakeup pins configured on PA0 and PC13 in this board which can be used to wake the device out of standby. 

If I write code to configure these two wake up Pins to wake up from the standby mode individually, the system works flawlessly. ie, in 2 separate runs (individually), if I set the corresponding bits EWUP1 (PA0) and EWUP2 (PC13) of PWR_CSR register and enter into Standby mode, whenever I perform a low to high transition on the corresponding pin, the system comes out of standby.

However, if both these are enable together simultaneously in the same code

(PWR_CSR|= (EWUP1_SET|EWUP2_SET) ) and I enter standby, only the EWUP2 (PC13) wakes the microcontroller up, not EWUP1 (PA0), even though ithis it is set before entering into standby. I have tried a number of ways, but it does not seem to be working.

Individually however, PA0 and PC13 works. Can somebody throw some light on what may be the reason?

This topic has been closed for replies.

1 reply

SKosh.3
SKosh.3Author
Associate
July 15, 2021

Can somebody help me with this? I am not able to get a clear answer of this