Skip to main content
GGonz
Visitor II
Feb 5, 2019 8:03 PM UTC
Question

Does the STM32H750 support multi-drop SWD?

Does the new STM32H750 MCU Family include the ARM CoreSight Serial Wire protocol version 2 in ADIv5.1 released in Sept 2009 which permits support for the multi-drop SWD extensions? The objective being the use of a single SWD debug header to enable debug of multiple MCUs whose SWD are interconnected.

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Feb 5, 2019 8:11 PM UTC

Some of the H7 parts support multiple "Access Ports" via the ST-LINK V3 connection

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Chief
Feb 5, 2019 8:27 PM UTC

STM32F7 and STM32H7 supports SWD version 2. So the MCU Idcode is already visible in the in the access port and so it should supports multi drop. Probably L5 will also be protocol version 2. Let's see.

Khouloud GARSI
ST Employee
Feb 6, 2019 10:37 AM UTC

Hi @GGonz​ ,

Indeed, the STM32H750 supports Serial Wire Debug protocol version 2, which provides a multi-drop capability.

Khouloud.