Skip to main content
sarang2
Associate
Oct 4, 2017 5:37 AM UTC
Solved

Does STM32L072 support USB programming/debugging?

Posted on October 04, 2017 at 07:37

Hello All,

Is it possible that STM32L072 can be programmed/debugged through USB?  It would be nice if somebody could share reference to the possible ways the micro-controller can be programmed/debugged.

Best Regards,

Sarang

#stm32l072
This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Oct 4, 2017 5:19 PM UTC
Posted on October 04, 2017 at 17:19

Debugging is effected by an external pod, not sure where the confusion is here. The NUCLEO/DISCO implementations include a secondary chip to provide the ST-LINK SWD connections.

One can program the device cheaply/effectively via a USART connection. You can also use serial as a highly effective means of providing debug and telemetry data.

Any debug via USB would need to be implemented by you, ie create a USB CDC or HID to exfiltrate the log data.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

3 replies

Tilen MAJERLE
ST Employee
Oct 4, 2017 5:41 AM UTC
Posted on October 04, 2017 at 07:41

Hello

Suryawanshi.Sarang

‌,

You can program STM32L072 using USB DFU mode with embedded bootloader, however directly debug option is not supported. In this case you need external programmer/debugger.

You can find more about DFU programming via USB here:

http://www.st.com/content/ccc/resource/technical/document/application_note/6a/17/92/02/58/98/45/0c/CD00264pdf/files/CD00264pdf/jcr:content/translations/en.CD00264pdf

Best regards,

Tilen

sarang2
sarang2Author
Associate
Oct 4, 2017 12:39 PM UTC
Posted on October 04, 2017 at 14:39

Hello Tilen,

Thank you for the prompt reply.

I understand that USB debugging(step debug) is not supported by STM32L072.

However I would like to confirm if I could get debug log through USB.

Best Regards,

Sarang

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Oct 4, 2017 5:19 PM UTC
Posted on October 04, 2017 at 17:19

Debugging is effected by an external pod, not sure where the confusion is here. The NUCLEO/DISCO implementations include a secondary chip to provide the ST-LINK SWD connections.

One can program the device cheaply/effectively via a USART connection. You can also use serial as a highly effective means of providing debug and telemetry data.

Any debug via USB would need to be implemented by you, ie create a USB CDC or HID to exfiltrate the log data.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..