Question
Does NUCLEO-H755ZI-Q Support Ethernet?
Hi everyone,
I'm using the NUCLEO-H755ZI-Q board and I’m a bit confused about its Ethernet support.
The user manual (MB1363 Rev C) shows that both H745ZI-Q and H755ZI-Q support Ethernet using the LAN8742A PHY. It also lists jumpers and solder bridge settings for enabling RMII.
But when I checked my H755ZI-Q board, it looks like the PHY chip and RJ45 connector are not soldered. So now I’m not sure:
Does the H755ZI-Q actually support Ethernet out of the box?
Or is Ethernet only available on the H745ZI-Q version?
Would appreciate any help or clarification. Thanks!