Skip to main content
Ala
Senior
May 1, 2022
Solved

Does micro detects low power?

hey there

I have a question: can a micro, say stm32f407 detect low power? for example is there a HAL function to indicate VDD lower that 3.3v?

(this way any time that power is going, I can for example save everything before power off)

This topic has been closed for replies.
KnarfB
KnarfBBest answer
Super User
May 1, 2022

You can measure Vdd in software using ADC and VREFINT. But there is no single HAL function doing everything for you. You can also use hardware features. Check for brownout reset (BOR) and/or programmable voltage detector (PVD) in the ref. man..

hth

KnarfB

2 replies

waclawek.jan
Super User
May 1, 2022

By measuring the internal voltage reference using ADC, you in turn determine voltage of VREF+. If you have that tied to VDDA and that one to VDD, you can detect decrease of VDD.

Similarly, if you don't use battery, you can connect VDD to VBAT and use the VBAT measurement in ADC to determine VDD decrease.

JW

KnarfB
KnarfBBest answer
Super User
May 1, 2022

You can measure Vdd in software using ADC and VREFINT. But there is no single HAL function doing everything for you. You can also use hardware features. Check for brownout reset (BOR) and/or programmable voltage detector (PVD) in the ref. man..

hth

KnarfB