Skip to main content
PB.4
Associate III
Feb 5, 2022 4:54 PM UTC
Question

Does it possible to write a byte of values to the flash memory of STM32F030CC

Hello all,

Can anyone in his forum to let me know whether can be write a byte in to the flash memory of the STM32F030CC uC, it always asking to increment the the write size as '4' bytes, if I hchange the code to write as a byte or even a two bytes the uC enter into hard fault handler, why? The code is below:

uint32_t Flash_Write_Data (uint32_t StartPageAddress, uint32_t *Data, uint16_t numberofwords)
{
	static FLASH_EraseInitTypeDef EraseInitStruct;
	uint32_t PAGEError;
	int sofar = 0;
 
	/* Unlock the Flash to enable the flash control register access *************/
	HAL_FLASH_Unlock();
 
	/* Erase the user Flash area*/
	uint32_t StartPage = GetPage(StartPageAddress);
	uint32_t EndPageAdress = StartPageAddress + numberofwords*4;
	uint32_t EndPage = GetPage(EndPageAdress);
 
	/* Fill EraseInit structure*/
	EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
	EraseInitStruct.PageAddress = StartPage;
	EraseInitStruct.NbPages = ((EndPage - StartPage)/FLASH_PAGE_SIZE) +1;
 
 
	 if (HAL_FLASHEx_Erase(&EraseInitStruct, &PAGEError) != HAL_OK)
	 {
		 /*Error occurred while page erase.*/
		 return HAL_FLASH_GetError ();
	 }
 
	 /* Program the user Flash area word by word*/
 
	 while (sofar < numberofwords)
	 {
		 if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, StartPageAddress, Data[sofar]) == HAL_OK)
		 {
			 StartPageAddress += 4; // use StartPageAddress += 2 for half word and 8 for double word
			 sofar++;
		 }
		 else
		 {
		 /* Error occurred while writing data in Flash memory*/
			 return HAL_FLASH_GetError ();
		 }
	 }
 
	 /* Lock the Flash to disable the flash control register access (recommended
		 to protect the FLASH memory against possible unwanted operation) *********/
	 HAL_FLASH_Lock();
 
	 return 0;
}

This topic has been closed for replies.

2 replies

KnarfB
Super User
Feb 5, 2022 5:33 PM UTC

The reference manual says:

"The main Flash memory can be programmed 16 bits at a time. The program operation is started when the CPU writes a half-word into a main Flash memory address with the PG bit of the FLASH_CR register set. Any attempt to write data that are not half-word long will result in a bus error generating a Hard Fault interrupt."

Programming 16 Bits work if you use FLASH_TYPEPROGRAM_HALFWORD in your above code.

If you have to write several small pieces of data repeatedly, you might want to look into eeprom emulation code.

hth

KnarfB

Tesla DeLorean
Guru
Feb 5, 2022 5:38 PM UTC

Cortex-M0 will fault if you do unaligned reads or writes.

`Write structures as blocks of words, or come up with a different strategy to write/journal data into Flash sector(s)

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..