Does anyone has already used the both SDMMC interfaces of the STM32U5 at the same time?
On a new product we plan to use an STM32U5 MCU to manage a Wireless (WiFi/BT) module and a micro SD card.
As the Wireless module has an SDIO interface we have to use the both SDMMC interfaces of the STM32U5.
Does anyone has already done this kind of stuff? Even on another STM32.
We plan to produce a prototype board and test it with the module and the micro SD card.
But, I'm afraid that there is some incompatibility between SDIO and SD protocol when they are used at the same time.
Or some unexpected limitation.