Skip to main content
MNapi
Senior II
June 10, 2024
Question

Does anybody have working write routine for OSPI ? STM32H7 MX25LM51245G

I used this

BSP_OSPI_NOR_Write(uint8_t* pData, uint32_t WriteAddr, uint32_t Size) from

https://github.com/STMicroelectronics/stm32-external-loader/blob/main/STM32L4x_boards/MX25LM51245G_STM32L4P5G-DK/Sources/Library/stm32l4p5g_discovery_ospi_nor.c

 

but what happens after executing write I cannot access the H7 chip anymore.

I have to connect Boot0 pin to 3.3V then I can erase the internal FLASH in Cube programmer.

and it works again

 

uint8_t BSP_OSPI_NOR_Write(uint8_t* pData, uint32_t WriteAddr, uint32_t Size)
{
OSPI_RegularCmdTypeDef sCommand;
uint32_t end_addr, current_size, current_addr;

/* Calculation of the size between the write address and the end of the page */
current_size = MX25LM51245G_PAGE_SIZE - (WriteAddr % MX25LM51245G_PAGE_SIZE);

/* Check if the size of the data is less than the remaining place in the page */
if (current_size > Size)
{
current_size = Size;
}

/* Initialize the adress variables */
current_addr = WriteAddr;
end_addr = WriteAddr + Size;

sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;

sCommand.FlashId = HAL_OSPI_FLASH_ID_1;
sCommand.Instruction = OCTAL_PAGE_PROG_CMD;
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_8_LINES;
sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_16_BITS;
sCommand.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_DISABLE;
sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_DISABLE;
sCommand.AlternateBytes = 0x00;
sCommand.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
sCommand.AlternateBytesSize = HAL_OSPI_ALTERNATE_BYTES_8_BITS;
sCommand.AlternateBytesDtrMode = HAL_OSPI_ALTERNATE_BYTES_DTR_DISABLE;
sCommand.DataDtrMode = HAL_OSPI_DATA_DTR_DISABLE;
sCommand.DummyCycles = 0;
sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;

sCommand.Instruction = OCTAL_PAGE_PROG_CMD;
sCommand.AddressMode = HAL_OSPI_ADDRESS_8_LINES;
sCommand.AddressSize = HAL_OSPI_ADDRESS_32_BITS;

sCommand.DataMode = HAL_OSPI_DATA_8_LINES;


/* Perform the write page by page */
do
{
sCommand.Address = current_addr;
sCommand.NbData = current_size;

/* Enable write operations */
if (OSPI_NOR_WriteEnable(&OSPINORHandle) != OSPI_NOR_OK)
{
return OSPI_NOR_ERROR;
}

/* Configure the command */
if (HAL_OSPI_Command(&OSPINORHandle, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return OSPI_NOR_ERROR;
}

/* Transmission of the data */
if (HAL_OSPI_Transmit(&OSPINORHandle, pData, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return OSPI_NOR_ERROR;
}

/* Configure automatic polling mode to wait for end of program */
if (OSPI_NOR_AutoPollingMemReady(&OSPINORHandle, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != OSPI_NOR_OK)
{
return OSPI_NOR_ERROR;
}

/* Update the address and size variables for next page programming */
current_addr += current_size;
pData += current_size;
current_size = ((current_addr + MX25LM51245G_PAGE_SIZE) > end_addr) ? (end_addr - current_addr) : MX25LM51245G_PAGE_SIZE;
} while (current_addr < end_addr);


return OSPI_NOR_OK;
}

This topic has been closed for replies.

7 replies

Tesla DeLorean
Guru
June 10, 2024

Is it stuck in OSPI_NOR_AutoPollingMemReady(), error or timeout?

If it is left active there will be problems, check the exit paths, if it doesn't complete with a match you'll need to use HAL_OSPI_Abort() to stop it.

 

>>but what happens after executing write I cannot access the H7 chip anymore.

Your code probably starts, but gets stuck later. Instrument better so you can see how far it gets before locking up.

Does the OCTOSPI device have it's own async reset input?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MNapi
MNapiAuthor
Senior II
June 10, 2024

No it does not stock in OSPI_NOR_AutoPollingMemReady()

 

I had this problem and I found solution. Actually I have it all working fine in Keil.

I try now CubeIDE, I can erase, read

all those functions work fine

/* USER CODE BEGIN 2 */

OSPI_NOR_OctalMode(&hospi1, OSPI_NOR_OCTAL_ENABLE);

OSPI_NOR_WriteEnable(&hospi1);

OSPI_NOR_Erase_Sector( 0x1000, 0x2000);

 

/* USER CODE END 2 */

It is not freezing it will not write to the memory, it gets to while(1) loop and it is working fine

After that when I try to access the chip to upload code it says no STM32 target

The function to write from this github does not work and it makes the chip inaccessible after executing but not freezing. They have the code for Ewarm, maybe it has something to do with compiler itself.

Tesla DeLorean
Guru
June 10, 2024

Inaccessibility by STM32 Cube Programmer (without external loaders) points more to a LDO/SMPS issue, or PA13/PA14 being reconfigured. Or a bus level issue.

Not sure it would be a compiler thing, the IDE's use their own external loaders, not ST's

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
LCE
Principal III
June 11, 2024
/* +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ */
/* OCTOSPI FLASH write page
 *	in SPI OCTAL mode
 */
/**
 * @brief write page - SPI or MULT
 *				### BLOCKING ###
 *				but only takes about 20µs at 50 MHz,
 *				waiting for programming page done in state machine
 * @PAram none
 *				write settings elsewhere,
 *				for now fixed page buffer is used
 * @retval 0 = ok
 */
uint8_t OspiFlashWrPage(void)
{
	uint8_t u8RetVal = 0;

	/* check pointer */
	if( NULL == sOspiFlashCtl.pu8WrBuf )
	{
		#if DEBUG_OSPIFLASH
			uart_printf("# ERR: OspiFlashWrPage(): pu8WrBuf = NULL\n\r");
		#endif 	/* DEBUG_OSPIFLASH */
		return HAL_ERROR;
	}

	/* check if flash shows write in progress */
	if( OspiFlashCheckSrWip() != 0 )
	{
		#if DEBUG_OSPIFLASH
			uart_printf("# ERR: OspiFlashWrPage(): WIP\n\r");
		#endif 	/* DEBUG_OSPIFLASH */
		return HAL_ERROR;
	}

	/* check SPI / OCTAL STR mode */
	u8RetVal = OspiFlashRdRegCR2();
	if( HAL_OK != u8RetVal )
	{
		#if DEBUG_OSPIFLASH
			uart_printf("# ERR: OspiFlashWrPage(): OspiFlashRdRegCR2()\n\r");
		#endif 	/* DEBUG_OSPIFLASH */
		return HAL_ERROR;
	}
	else if( (0 != sOspiFlashRegs.u8CR2) &&
			 (0 == (sOspiFlashRegs.u8CR2 & OSPI_FLASH_CR2_SOPI)) )
	{
		#if DEBUG_OSPIFLASH
			uart_printf("# ERR: OspiFlashWrPage(): not in SPI or MULT mode\n\r");
		#endif 	/* DEBUG_OSPIFLASH */
		return HAL_ERROR;
	}

	/* set write enable */
	if( OspiFlashWriteEnable() )
	{
		#if DEBUG_OSPIFLASH
			uart_printf("# ERR: OspiFlashWrPage(): OspiFlashWriteEnable()\n\r");
		#endif 	/* DEBUG_OSPIFLASH */
		return HAL_ERROR;
	}

	/* wait for internal BUSY release to write registers */
	if( OspiFlashCheckBusyTo(OSPI_FLASH_TO_BUSY_MS) )
	{
		#if DEBUG_OSPIFLASH
			uart_printf("# ERR: OspiFlashWrPage(): OCTOSPI_SR_BUSY\n\r");
		#endif 	/* DEBUG_OSPIFLASH */
		return HAL_ERROR;
	}

/* +++++++++++++++++++++++++++++++++++++++++++ */
/* command config */

	/* CR: functional mode = 00 = indirect WRITE */
	pOspiFlash->CR = OSPI_FLASH_CR_EN_IWRITE;
	/* CCR: reset */
	pOspiFlash->CCR = 0;
	/* DLR: data length */
	pOspiFlash->DLR = (sOspiFlashCtl.u32WrLen - 1);
	/* AR: set address */
	pOspiFlash->AR = sOspiFlashCtl.u32WrAddr;

	if( OSPIFLSH_MODE_SPI == u8OspiFlashMode )
	{
		/* TCR: SPI write dummy cycles between addr and data */
		pOspiFlash->TCR = OSPI_FLASH_TCR_SPI_STR;
		/* CCR: no DTR, SPI 8b instruction + 8b data + 32b address: 1 line */
		pOspiFlash->CCR = OSPI_FLASH_CCR_SPI_STR_D1A32I8;
		/* IR: set write instruction */
		pOspiFlash->IR = OSPI_FLASH_CMD_SPI_WR_DATA_4BA;
	}
	else if( OSPIFLSH_MODE_MULT == u8OspiFlashMode )
	{
		/* TCR: OCT write dummy cycles between addr and data */
		pOspiFlash->TCR = OSPI_FLASH_TCR_OCT_STR_WR_DAT;
		/* write data in OCTAL mode with 4 byte address */
		pOspiFlash->CCR = OSPI_FLASH_CCR_OCT_STR_D8A32I16;

		/* IR: set write MULT STR instruction */
		pOspiFlash->IR 	= OSPI_FLASH_CMD_MULT_PROG_PAGE;
	}
	else
	{
		#if DEBUG_OSPIFLASH
			uart_printf("# ERR: OspiFlashWrPage(): not in SPI or MULT mode\n\r");
		#endif 	/* DEBUG_OSPIFLASH */
		return HAL_ERROR;
	}

/* command config done */
/* --------------------------------------------- */

#if DEBUG_OSPIFLASH
	uart_printf("pOspiFlash->DLR = %08lX\n\r", pOspiFlash->DLR);
	uart_printf("pOspiFlash->TCR = %08lX\n\r", pOspiFlash->TCR);
	uart_printf("pOspiFlash->CCR = %08lX\n\r", pOspiFlash->CCR);
	uart_printf("pOspiFlash->IR = %08lX\n\r", pOspiFlash->IR);
	uart_printf("pOspiFlash->AR = %08lX\n\r", pOspiFlash->AR);
	uart_printf("sOspiFlashCtl.u32WrLen = %lu\n\r", sOspiFlashCtl.u32WrLen);
#endif 	/* DEBUG_OSPIFLASH */

/* +++++++++++++++++++++++++++++++++++++++++++ */
/* transfer with command, address & data
 *	TRIGGER: writing data register OCTOSPIn->DR
 */

	/* get data via pointer for byte cast */
	__IO uint32_t *pu32DR = &pOspiFlash->DR;

	for( uint32_t i = 0; i < OSPI_FLASH_PAGE_SIZE; i++ )
	{
		u8RetVal = OspiFlashWaitFlagSetTo(OCTOSPI_SR_FTF, OSPI_FLASH_TO_WRFF_MS);
		if( u8RetVal != 0 ) break;

		/* write byte to flash */
		//*((__IO uint8_t *)pu32DR) = u8OspiFlashPageBuf[i];
		*((__IO uint8_t *)pu32DR) = sOspiFlashCtl.pu8WrBuf[i];
		sOspiFlashCtl.u32WrBtDone++;
	}

/* writing data done */
/* --------------------------------------------- */

	/* check transfer complete */
	if( OspiFlashWaitFlagSetTo(OCTOSPI_SR_TCF, OSPI_FLASH_TO_WRFF_MS) )
	{
		u8RetVal++;
		#if DEBUG_OSPIFLASH
			uart_printf("# ERR: OspiFlashWrPage(): OCTOSPI_SR_TCF, u32WrBtDone = %lu\n\r", sOspiFlashCtl.u32WrBtDone);
		#endif 	/* DEBUG_OSPIFLASH */
	}
	#if( 0 ) //DEBUG_OSPIFLASH
		else uart_printf("OspiFlashWrPage() okay, u32WrBtDone = %lu\n\r", sOspiFlashCtl.u32WrBtDone);
	#endif 	/* DEBUG_OSPIFLASH */

	/* clear transfer complete flag */
	pOspiFlash->FCR = OCTOSPI_FCR_CTCF;

	/* transfer ERROR check */
	if( pOspiFlash->SR & OCTOSPI_SR_TEF )
	{
		u8RetVal++;
		u32OspiFlashErrTE++;
		/* clear register flag */
		pOspiFlash->FCR = OCTOSPI_FCR_CTEF;
		#if DEBUG_OSPIFLASH
			uart_printf("# ERR: OspiFlashWrPage(): OCTOSPI_SR_TEF\n\r");
		#endif 	/* DEBUG_OSPIFLASH */
	}

	return u8RetVal;
}

 

No HAL, but working...