Do the G4 series contain a DMA on timer break feature?
The RM0440 ch. 28.3.18 rev7 mentions on page 1128:
> An interrupt is generated if the BIE bit in the TIMx_DIER register is set. A DMA request can be sent if the BDE bit in the TIMx_DIER register is set.
Unfortunately, the DIER register does not contain a BDE bit. Additionally there is no DMA line available for the break (unless it uses the TIM_TRIG line).
Is this sentence a remnant from initially planned features, or are the other parts just missing?