Question
Do I need to compile different binaries for two MCUs in the same family that only differ in flash size?
I have an STM32F427VGT6 and a STM32F427VIT6 which only differ in Flash size. I have firmware that works fine on the variant with smaller flash size. Do I need to recompile it for the larger variant or will I be able to flash it as is?
I am asking because we're trying to evaluate the larger version as a drop in replacement in case sourcing is more difficult.