Skip to main content
RGris
Associate II
August 23, 2019
Question

Do ADCs have independent input channels in dual mode?

  • August 23, 2019
  • 5 replies
  • 1159 views

I want to use ADC1 and ADC2 in dual mode simultaneous. In reference manual on p.360 there is a note that states that i can't convert tha same channel on both ADCs simultaneously ("no overlapping sampling times for the two ADCs when converting the same channel"). In my case on both ADCs channels 1 and 3 are used, but the channels of ADC1 and ADC2 are (as usual) mapped to different pins. Why can't I convert simultaneously ADC1_CH1 and ADC2_CH2 if these channels are phisically different and each ADC has it's own sampling circuit? Do ADCs have independent input channels in dual mode or share some common set of channels?

This topic has been closed for replies.

5 replies

Olivier GALLIEN
ST Technical Moderator
August 26, 2019

Hi @RGris​ 

Can you please specify which STM32 you are using ?

Thx

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
RGris
RGrisAuthor
Associate II
August 26, 2019

STM32F303CC

RM

Olivier GALLIEN
ST Technical Moderator
August 26, 2019

Thanks, remove topic "STM32 MPUs" then and add STM32F3.

This should help to reach relevant people for support.

BR

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
RGris
RGrisAuthor
Associate II
August 26, 2019

Olivier as far as I concern this quastion already has topic "STM32F3"

Sould I remove "STM32 MCUs" (not MPU)?